IP.MODE
Description
This parameter is used to determine how the drive acquires an IP address for service port communication.
Examples
Usage
1: A static IP address is defined by the value set using IP.ADDRESS
2 (default): Acquire a dynamic IP address using DHCP or Auto-IP. If a DHCP server is not available, the drive will use Auto-IP to identify and acquire an available IP address.
Code
Set drive to use static IP of 192.168.0.1
--> IP.MODE 1
--> IP.ADDRESS 192.168.0.1
--> IP.SUBNET 255.255.255.0
--> IP.RESET
Context
For more information on IP configuration, refer to Finding and Connecting to a Device.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 1 to 2 |
| Default Value | 2 |
| Data Type | Integer |
| See Also | IP.ADDRESS, IP.SUBNET, IP.GATEWAY, IP.RESET |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants supported
Fieldbus Information
|
Copyright © 2018 Kollmorgen |
|